Other Parts Discussed in Thread: LM5149-LM25149DESIGN-CALC, LM5149
We are currently prototyping a power supply with an input of 48V and an output of 25V and 8A.
Set constants using LM5149-LM25149DESIGN-CALC.
I am aiming for stable operation with a simple circuit.
AEF (No Input Filter)
UVLO 35V-30V
DITHER Disabled
FPWM (Tie PFM to GND)
External Compensation




I have inserted a 1kΩ and 0.1uF filter into ISNS+.
It operates stably at 150kHz when the load current is around 3A, but the oscillation frequency drops to about 20kHz when the load is less than 2A or more than 4A. The current amplitude increases, saturating the inductor and destroying the FET.
Could you please advise me on the cause of the frequency change?