This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP3878-ADJ: I'm looking for replacement parts.

Part Number: LP3878-ADJ

Hi TI team

LP3878MRX-ADJ/NOPB will be discontinued, so I am looking for replacement parts.

Since Re-Artwork is difficult, is there an alternative part with the same Pin Configuration and Package?

The required specifications are as follows.

 Input Voltage: 2.5 to 3.3 V, Voltage margin is also required.

Output Voltage: 1.2V or 1.8V or 2.5V, It is okay even if the Output Voltage is fixed.

Thanks and Best Regards,

Akira Ono

  • Hello Akira, 

    Thank you for your question! Unfortunately, we don't have any p2p alternatives for this device. The closest match is going to be TLV76701DGNR, it has a 1A input current range. 16V Vin range with improved accuracy and PSRR. Let me know if you have any additional questions. 

    Thanks, 

    McKyla