Hi,
I've uploaded your model into LTSpice and simulated it to understand the EN pin configuration.
The EN pin follows the IN voltage if <6.5V and is clamped to 6.5V by an internal zener.
I want to control the TPS709 operation by external voltage through the N-Channel FET that pulls down the EN pin to disable the regulator.
I see it's working well in simulation, but would like to understand if this is an acceptable control type. Do I need to limit the current from the EN pin to GND when disabling it (pulling low) with some external resistor or it's limited internally by a 300nA current source?