Hi,
The following questions assume that USB is always connected after USB was connected and IC started charging.
1. If VBUS_STAT changes 010→000→010 after charging starts, will the REG0D register return to the Default value? Is it necessary to reconfigure the REG0D at this time?
2. If charging starts and VBUS_STAT is always 010 and PG_STAT changes 1→0→1, will the REG0D register return to the Default value? Is it necessary to reconfigure the REG0D at this time?
3. In addition to the above, please tell me the case where the REG0D register is expected to return to the default value when the USB cable is continuously connected.
Best Regards,
Nishie