Other Parts Discussed in Thread: PMP22650, LMG3522R030
Hi there,
I am checking the documentation for the (TIDM-02013 7.4-kW on-board charger reference design with CCM totem pole PFC and CLLLC DC/DC using C2000 MCU)
evaluation board and I see that at the hardware level it is the same documentation supplied in Altium at the (PMP22650 GaN-based, 6.6-kW, bidirectional, onboard charger reference design)
evaluation board. Is this correct? If so, only the firmware changes?
Regarding to the documentation of the TIDM-02013 power board, which is the same as the PMP22650 in terms of HW, I see that the gerbers are incomplete, the intermediate layers (2,3,4,5,6 and 7) have not been generated, the design is 8 layers What is the reason for this lack of information?
Last question, Has anyone manufactured this evaluation board by themselves? What was the result? Was it difficult to get it going? I have read that some components such as inductors are difficult to get...
Thanks
Juan Carlos