Hello everyone,
I want to convert 12V to 5V using the TPS562200.
I have attached the schematic via the link below.
I initiate the simulation with a Stop Time of 10ms in Transient, but I encounter the error provided in the link below.
I have included the library as code, and I create the component by selecting 'create symbol' from the 'open' tab.
What do you think could be the issue? I've searched but couldn't find a solution. If you need more information, i can give more info.
Thank you.