Part Number: BQ2982
Other Parts Discussed in Thread: BQ21040, BQ25170
Hi team,
Our customer designed below battery management system using bq298216, CSD87501 and bq21040.
And they are evaluating this system in low battery voltage(VBAT) condition. BQ298216 has UVP function and UVP value is 2.5V. But when they started charge with Charge Voltage is 5V and VBAT is 2.1V condition, battery was charged with fast-charge current. They checked the charge current was constant fast-charge current(around 90mA) by both side voltage of Rsns.
Our understanding is that when VBAT is below 2.5V, UVP is enabled and battery is not charged and discharged.
Is this understanding correct? If you have any possible causes this behaver, please let me tell.
below figure is simply schematic, and next is waveform of VBAT and VOUT when supplied charging voltage 5V.


Best regards,
teritama