Hi,
I would like to know the exact ADC count to mV conversion for Analog channels.
CFETOFF
DFETOFF
TS1
TS3
HDQ
DCHG
DDSG
Its configured as 0x33
PIN_FXN[1 0] 11 = ADC Input or Thermistor
OPT[1:0] 00 = general purpose ADC input
OPT[3:2] 11 = no polynomial is used, raw ADC counts are reported
OPT[5:4] 00 = selects 18-kOhm pull-up for thermistor measurement
Below is my observation I am not able to convert ADC count to mV accurately, can you please guide me?
| Resistance Ohm | ADC Count | mV |
| 9500 | 462 | |
| 9500 | 470 | |
| 470 | 91 | |
| 330k | 1144 |

Based on the below diagram considering ref voltage as 1.8 and pull up resistance as 18k I tried to calculate as shown in image but I do not think it near by to expected value.

Regards,
Kishor