Hello Sir/Mam
We are using part TPS54A24RTWR to generate multiple voltages in our Design , But as we don't have it's average model we cannot run frequency response to check stability of system.
So, Please review the schematics once , compensations and input output capacitors.
Vin= 5V
Vout=0.92V
Iout=8.2A
Ac Ripple=10mV pk-pk
Dc Ripple= 2%
Vin= 12V
Vout=3.7V
Iout=9.6A
Ac Ripple=4 %
Dc Ripple= 4%
Vin= 12V
Vout=1.5V
Iout=7A
Ac Ripple=2 %
Dc Ripple= 1%