This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM27762: LTSpice error when generating negative voltage

Part Number: LM27762
Other Parts Discussed in Thread: PSPICE-FOR-TI

My goal is to generate +3V and -3V using this component. However when EN- is high (negative voltage active), the simulation fails and errors out after a bit. PGOOD is also high when it should be 0V. As far as I can tell, the capacitor values and resistor values I have chosen are correct as per the datasheet.

Any help is very much appreciated.