Part Number: BQ25176M
When a fault condition is detected STAT pin blinks at 1 Hz. When input supply 4.52v and battery voltage 3.48v for 1 cell LiIon 4.20 V and 500mA.
What kind of fault ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Saw
Sorry but could not read value for R10 and R11, what values are you using?
Schematic looks OK.
Both LEDs on would indicate Power is good (PG) and charge is in progress (STAT).
Check the voltage on ISET this will indicate what the charge current is.
Hello
ISET of 604 ohm will set charge current to 500mA, this is good.
VSET of 27.4k will set charge voltage to 4.2V this is good also.
In the test set up do you possibly have a current better between charger and battery? This has caused problems with other customers.