Other Parts Discussed in Thread: LM5155
Hi ...
I am working on the design in SEPIC based on the LM5157 and I am experiencing some problems. Let me start by saying that the circuit is going to have an input between 7.0 V to 20.0 V and the intention is for it to have an output voltage capability of 15.0 V and a current of 3.0 A. Is this feasible for the device?