This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25170: KSET Parameter Variability

Part Number: BQ25170


Hello,

We are running worst case analysis on the bq25170 with KSET varying from 270 - 330 we calculate needing approximately a 715 ohm resistor.

The issue is the wide ranging currents.  We calculate out with 715 ohms a 374mA_min and 467mA_max.

Are we running these calculations properly? 

Thank you, Keith