Hi,
I am planning to design a Step-Down circuit using the LMR43610MB3RPER.
Vin: 4.8~36V
Vout: 3.3V
Iout: 0.3A
Ripple Current Ratio K = 0.3

Using the inductor calculation formula provided in the datasheet, I found that when Vin is 4.8V, it's approximately 11uH, and when Vin is 36V, it's about 33uH.
-
In this case, which value should I choose between 11uH and 33uH? (For reference, designing with WEBENCH yielded a value of 8.2uH.)
-
Looking at the inductor specs selected by WEBENCH, it seems over-specified compared to the current consumption (0.3A) of the application I intend to use. Is there a reason for this?