This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62560: Peak output current

Part Number: TPS62560

Hi team,

My customer want to know current limit in datasheet.

1. 7.1 Absolute Maximum Ratings shows Peak output current is internally limited. 

Is this limit fixed value? If so, please teach me.

Or is this limit value the same as the ILIMF of the power switch between 0.8 and 1.2A?

2. Here is their TPS62560 output (3.3V) waveform.

On red circle, it seems that there are 3 times current limit. I think this behavior is due to charge of output capacitance, so this waveform is no problem. Is my understanding correct?

Regards,

Youhei MIYAOKA