Other Parts Discussed in Thread: BQ25713,
In looking at the comparison chart I see that the only difference between the BQ25713 and the BQ25713B is in the "Device Address" field.
BQ25713 = 6Bh
BQ25713B = 6Ah
What is the difference between the two?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Tim,
Your observation is correct. The two devices are basically the same except for the device address.
Best Regards,
Munir
Our customer has a call-out for the BQ25713 (6Bh) and the BQ25713B (6Ah) was ordered. We need to understand if using the "B" version will cause issues or if it is simply a matter of enhanced functionality over the "non-B" version.
Hi Tim,
Both of the them are the same chip except that the I2C addresses are different. BQ25713 has address 6Bh while BQ25713B has address 6Ah for I2C communication.
And yes they are interchangeable.
Best Regards,
Munir