This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC2842: Any methods to cool down the device temperature?

Part Number: UC2842


Hi team,

Our customer is now using UC2482 to their fly back power supply and frequency is 60kHz. 

But they found that the temperature of UC2482 raise about 50°C in room temperature, and the MOS fly back power supply also rasie too much.

Is there any way to make the rasing of temperature smaller?

Thanks,

Meng Zhen

  • Hi,

    Please check the VCC voltage and make that voltage closer to 12V say 15V.

    Also check your MOSFET gate charge to see if it demands a high driving power, and if so, you need to add external driver, such as a totem pole, or change the MOSFET with smaller gate charge.