This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25942L: TPS25942L heat generation calculation

Guru 14090 points

Part Number: TPS25942L

Hi,

I'm considering using the WQFN package for TPS25942L. The current consumed by the TPS25942L is large and I am concerned about heat generation. I would like to check how to calculate the theoretical maximum heat value of TPS25942L. Am I correct in my understanding that if the P[W] of the IC exceeds 2.7W from Tj= (θja x P) + Ta = ( 38.1[℃/W] x P[W] ) + 25℃, it is difficult to use the TPS25942L from the standpoint of heat generation?

Thanks,

Conor