Hello,
could you pls simulate the LM5249-Q1 and tell me the exact accuracy of line regulation and load regulation?
The configuration is shown below, thank you for your support!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
could you pls simulate the LM5249-Q1 and tell me the exact accuracy of line regulation and load regulation?
The configuration is shown below, thank you for your support!
Hello,
This has been assigned to Orlando. Please expect to here back from him here.
Regards,
Jimmy
Mingkang,
We cannot give exact load/line regulation for the system.
On your board you can have variances due to layout or noise.
In ideal cases the load regulation should be close to 0.1% and the line regulation should 1%
You can see this in our EVM, LM5149-Q1EVM-400.
Also remember that PFM mode will have higher output voltage ripple.
Hope this helps,
-Orlando
Hi Orlando, thanks for your reply!
When we tested the inductor ripple current, we found that there was a periodic spike in the current flowing through the inductor. Please help analyze the cause. Thank you!
Input voltage: 24V/36V, Output voltage: 14.68 V, current: Around 1.2 A, current limit setting: 4 A (shunt: 15 mΩ)
1. at input voltage of 24V and 36V, respectively, there are current spikes at different intervals (36-V current spikes are spaced approximately 30 ms, 24-V is approximately 183 ms)
2.observe the details of the current waveform and the current change is in accordance with the set buck switching frequency (T=2.14us) as follows:
Supply voltage 36 V:
Supply voltage 24V:
Mingkang,
Not sure about the random spike intervals.
1. Is active EMI enabled? does this happen if you disable active EMI (CNFG to GND) ?
2. Can you run a bode plot to evaluate your bandwidth and phase margin?
I see the ringing frequency is close to 12kHz, that could be marginal instability and low phase margin.
-Orlando
Hi Orlando,
The Bode plot is as follows, both amplitude margin and phase margin should be sufficient.
Now we are using active EMI, later we will disable the active EMI and test. Why is active EMI likely to cause this problem?
Mingkang,
I mean measure the bode plot on board.
I wasn't sure if AEF would cause the problem, and it is easy to disable, however it is not causing the problem.
-Orlando
Thanks so much for your quick reply! Problem already solved, it's test condition related. :)