Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5117: LM5117 test issue

Part Number: LM5117

HI SIR

There are some problems with testing IC LM5117, please refer to the attachment.

TKS

LM5117 IC design and measurement issues_20240118.docx

  • Hello TKS 

    The cathode voltage of the DS404 can be greater than the input voltage only during transients when the input voltage falls down quickly. During normal operation, it is not possible to make the cathode voltage greater than 42V input voltage for a long time like as the screen capture in the DOCX file. 

    Please check if any signal or power rail is around the converter circuit, whose voltage is greater than the 42V.  

    -EL