Part Number: LM5148-Q1
Other Parts Discussed in Thread: LM5148, LM5149-Q1EVM-400
Hi Team,
This is regarding the buck converter Protection Circuit Design.
Input Voltage: 40V-60V
Output Voltage: 13.8V
Output Current: 10A (max)
Switching Frequency: 460-500kHz
Gate Voltage: 4.8V (when measured)
I have Designed an Overvoltage protection Using basic Crowbar Design for both Input as well as Output Using A Single SCR. There are other protection requirements like Overcurrent/Short Circuit Protection as well as Over Temperature protection. I am Stuck at thow to design the Overcurrent/ Short Circuit Protection. It would be helpful if there any low cost Solutions for the Over Current or Short Circuit Protection Regarding this Application.
Thanks & Regards,
Mahankali Nikhilindu Kasyap