The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5148-Q1: Protection Circuit Design

Part Number: LM5148-Q1
Other Parts Discussed in Thread: LM5148, LM5149-Q1EVM-400

Hi Team,

This is regarding the buck converter Protection Circuit Design.

Input Voltage: 40V-60V

Output Voltage: 13.8V

Output Current: 10A (max)

Switching Frequency: 460-500kHz

Gate Voltage: 4.8V (when measured)

I have Designed an Overvoltage protection Using basic Crowbar Design for both Input as well as Output Using A Single SCR. There are other protection requirements like Overcurrent/Short Circuit Protection as well as Over Temperature protection. I am Stuck at thow to design the Overcurrent/ Short Circuit Protection. It would be helpful if there any low cost Solutions for the Over Current or Short Circuit Protection Regarding this Application.

Thanks & Regards,

Mahankali Nikhilindu Kasyap