Dear Team,
Could you help to review the schematic as below?

Many Thanks,
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jimmy,
The BAT pin appears to be missing a 1 uF capacitor close to the IC as well as a 10 uF capacitor close to the SYS pin.
Additionally I'm trying to understand the interaction between USB5V and the VBAT-VBATT FET. It looks like VBATT will only be connected to VBAT when VIN voltage is present or when the on switch is connected. Is this a power saving method to manually disconnect the battery from the system?
Best Regards,
Juan Ospina
Hi Ospina,
Customer just want to know how to input the register to make sure Vbat at 4.2V to charge the battery.
Please support and reply. Thanks.
Hi,
To set VBAT regulation voltage to 4.2V, the customer will have to write VBAT_CTRL (Register 0x03) to 0x46. This is the default value of the register so the customer should not need any I2C transaction to see the behavior. It should charge to 4.2V by default.
Best Regards,
Juan Ospina
Hi Juan,
We appreciated your great support.
I try to remove the Q1, Q2 and let battery connected to charger and test the BQ21080 at no I2C and register setting.
I didn’t measure 4.2V on BAT,
Battery looks like charging but very slowly (3.79V to 3.81V for 1HR)
is this normal?
I would like to ask about the application of BQ21080 in the circuit.
When there is no I2C communication and Register is defaulted
Will the BAT pin have a 4.2V output?
Attached is our current circuit
Because the preliminary measurement is under the condition that there is no I2C communication and Register is defaulted
The BAT pin only has the voltage of the battery itself, It's 4V.
Many Thanks,
Jimmy
Hi Jimmy,
Attached is our current circuit
I think you may be missing an attachment.
Battery looks like charging but very slowly (3.79V to 3.81V for 1HR)
is this normal?
This depends on the battery size, do you know how many mAh the battery is? The default charge current for the charger is 10 mA so for a big battery it may take a long time to charge. This setting can be changed only through I2C communication.
When there is no I2C communication and Register is defaulted
Will the BAT pin have a 4.2V output?
Yes, the default register value for VBATREG is 4.2V so by default the charger should attempt to charge to 4.2V
Because the preliminary measurement is under the condition that there is no I2C communication and Register is defaulted
The BAT pin only has the voltage of the battery itself, It's 4V.
BAT pin will always be the voltage of the battery. As the battery gets charged it should rise to the regulation voltage (4.2V) minus a very small offset due to termination and any resistance voltage losses between the BAT pin and the Battery.
Best Regards,
Juan Ospina
Hi Juan,
Adding SYS is difficult due to PCB space
We are still trying to add SYS capacitor.
Just confirm, will it be affected if the SYS capacitor is not added? Thanks a lot.
Many Thanks,
Jimmy
Hi Jimmy
Without the SYS capacitor the device may have some stability difficulties. Although it may still charge the device hasn't been characterized without this capacitor so we can't guarantee the device behavior.
Battery looks like charging but very slowly (3.79V to 3.81V for 1HR)
is this normal?
Was the customer able to resolve this issue? I don't believe this would be caused by the missing SYS capacitor.
Best Regards,
Juan Ospina