Part Number: LMR50410-Q1
Hi Team,
My customer is using the LMR50410-Q1 in the On board charger. And they ask us if the RC filter at SW pin is ok to be added. I haven't clarify the reason why customer want to add this modification, but very likely it is for EMI performance improve.
Here is the schematic, and it is the 12V to 5V buck conversion.

Can you help to advise:
1. If that is ok to add the RC as above picture?
2. If yes, any consideration on the RC siziing?
Thank you!
Pin