This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS785-Q1: Regarding taping specification

Part Number: TPS785-Q1

Hi team,

Would your please let us know taping specification for TPS78518QWDRBRQ1 ?

Our customer wants to know for automatic manufacturing with state of taping reel.

Information Request

Reel dimensions : diameter and width

Taping dimensions : A0, B0, K0, W, P1 and Pin1 Quadrant (Q3 right?)

Best regards,

Yusuke Kawate

TED

  • Hi Kawate-san,

    This information should be found in the datasheet under "TAPE AND REEL INFORMATION" for all of our products, but I checked and noticed that it is not included for SON-8 package orderables on the datasheet. I have alerted the appropriate team, and we're working to get that resolved.

    For TPS78518QWDRBRQ1, please see below table for requested information until the datasheet is updated:

    Spec Value
    Reel Diameter 330mm
    Reel Width 12.4mm
    Tape Dimension A0 3.3mm
    Tape Dimension B0 3.3mm
    Tape Dimension K0 1.1mm
    Tape Dimension W 12mm
    Tape Dimension P1 8mm
    Pin 1 Quadrant Q3

    Regards,

    Kelsey

  • Dear Kelsey san,

    Thank you for your kind and prompt reply.

    I understood above information and will annouce to our customer.

    Best regards,

    Yusuke Kawate

    TED