This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92691: TPS92691QPWPRQ1 Soft Start Issue

Part Number: TPS92691


Hello, 
I am using the TPS92691QPWPRQ1 driver to control the backlight of a panel. 
As there are some timing that are required in order to power up the panel i need to introduce some delay in the backlight voltage. 

The way I try to do it, is to put a large capacitor on the soft start time, but it seems that at it is not properly used in my application and I am trying to find if it is normal behavior or not. 

Please see the green signal from the picture below. The internal circuitry of the panel is pulling down all the signals for a short time and them bring them HIGH with a defined power up sequence. 

The green signals should start about 2.5 or 3S from the yellow line (when it is high); 

What I can see is that the green signals is kept at mid level and after 3s it goes high. 
Is there a way to keep the signal low till 3S after the yellow signals for example?