Hello,
I am planning to use TPS63710 to obtain -3.3V from a 5V input. According to the datasheet, as long as 5V > 0.7x|3.3V|,
there should be no issues. Please confirm this for me.
I am currently using the TPS63710 to generate a -2.5V output from a 5V input.
To achieve a -3.3V output in the circuit diagram above, can I change R1 (R402) to 287K and R2 (R403) to 150K?
Thank you