Hi Team,
CSD19502Q5B VGS=10V, ID=50A Drain-source on-state resistance can under 3mΩ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
CSD19502Q5B VGS=10V, ID=50A Drain-source on-state resistance can under 3mΩ?
Hello Kevin,
Thanks for your interest in TI FETs. The CSD19502Q5B max Rds(on) = 4.1mΩ at VGS = 10V. It is our lowest on resistance 80V NFET in 5x6mm SON package. This is slightly higher than the competition which is 3mΩ max at VGS = 10V. Let me know if you have any additional questions.
Best Regards,
John Wallace
TI FET Applications