This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi support team.
I am considering a circuit that generates positive and negative power supplies.
I thought of a Flubuck converter as the smallest circuit that could be designed, and I thought it might be possible to design it with this device that has an FPWM function.
A brief outline of the circuit is below.
Input voltage: 5V-15V
Output voltage: ±18V
Output current: 1A
Do you think it's possible?
However, the current challenge is not finding the optimal coupled inductor or Flybuck transformer. If you have any products you can recommend, please let me know.
It would be very helpful if you could tell me what is possible with other products if it is possible with this device.
Best regards,
Higa
Hello
I think that your output current of 1A is somewhat large for a fly-buck.
You may want to look more at a conventional fly-back design.
You may also want to look on the TI website for complete designs for your particular application.
Thanks
Hello
I will close this post.
If you need more help, please open a new post.
Thanks