Other Parts Discussed in Thread: LM5158
Hi
The SEPIC circuit was constructed and designed with the following specifications.
However, problems arise under the following conditions.
-SPEC-
INPUT: 8~36Vdc
Output: 24.7V or 12.85V (Set the voltage depending on whether the R38 resistor is inserted or not.)
-Question-
1. If the output voltage is set to 24.7v without inserting R38, noise occurs at an input voltage of 26V or higher and heat is generated severely.
2.If the output voltage is set to 12.85v, the input voltage will operate up to 36v without any problems
3.Why are the above two problems happening? Is there a solution?
Please review the circuit diagram below.
Thanks