Part Number: TUSB546EVM
Other Parts Discussed in Thread: TPS65982
Hello TI support,
I have a question regarding to the evaluation Board TUSB546EVM. We have a fixed setup where we want to connect a touchscreen to a PC through the evaluation Board.

Our Setup:
- Touchdisplay
- USB Type-C: Power (5V/2A), display and touch signals
- PC
- USB3.1 Type A
- Displayport
We tried the delivered EVM jumper configuration and the jumper configuration shown in the EVM manual. In each configuration the Power LED of the touchscreen lights up shortly and then switches off. I measured VBUS on the USB Type-C connection and noticed a toggling between 5V and 0V. The voltage of the USB Type-B connected is stable at 5V.
I have tested following:
- The touchscreen works with a direct USB Type-C connection from a standard laptop.
- Even if the touchscreen is only powered with 5V via a USB charger, at least the starting screen of the touchscreen appears.
- An USB flash drive connected to the TUSB546EVM works and it accessible through the PC.
It seems that the voltage from the USB Type-B is not being forwarded by the TPS65982 chip. Does the EVM board have a standard current limiter below 2A or is the problem caused by a different reason?
Thank you for your help