Other Parts Discussed in Thread: LM5157
Hi,
I need a suggestion for the isolated DC to DC conversion design with the below required specifications. Could you please suggest me a suitable design. Alternative part number is also fine...!
Input:
20V to 36VDC
Output:
+12V @ 0.8A
-9V @ 0.4A