Other Parts Discussed in Thread: BQSTUDIO
Hello,
Background: FS file based on a new battery with a reserve capacity of 350mAh.
Using a new battery, load the FS file made based on the new battery.
Different charging current 200mA and 1A。There will be a large change in TRUE FCC, and the True Fcc change is almost the same。
1、Please analyse the logs to see what caused the drastic change in the TRUE FCC?
2、Why does the TRUE FCC change by the same amount for different SOH batteries?
3. Is the above problem, related to FS files?Which specific configuration is the problem?
Attached is the log grabbed using TI demo board + BqStudio.
TI Demo+Bqstudio,True Fcc Test.zip6064.0418_New_Bat_FS_withChemID_0419.gm.zip