Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61391: Maximum Current Output

Part Number: TPS61391

Hello Team,

A design requires a voltage of ±80V to power an amplifier. Looking at the TPS61391 datasheet and EVM, it seems this part will work.

If I'm using the EVM as reference and outputting ±80V, what's the maximum output current the device can support? Figure 2 in the datasheet says the maximum current is 8mA at ~40V.

Is this true at 80V? Should we expect similar currents at -80V?

Regards,

Josh