Other Parts Discussed in Thread: LM5101C, UCC27211, UCC27211A, LM5101A, UCC27288, UCC27301A-Q1
Dear all,
Background:
My customer now are designing a 4 switched Buck-Boost converter. And they are using UCC27282 as the gate driver.
To achieve 100% duty cycle for the upper MOSFET. They connected a 12V isolated power supply in the HB(+) and the HS(-)
Experiments:
They have soft-start algorithm that duty cycle of the upper MOSFET will gradually increased with the scale of 1%, frequency is 120K, total time 65ms.
The steady operation stage will be the upper MOSFET consistently conducted which means 100%D and the lower MOSFET will off.
Once they let the output current up to 0.4A, failure will existed. I asked them to test the PIN. They found that the HB is shorted to the VSS.
other information:
input voltage 10-80V, output current max:20A, power:800W
yellow: converter output current Green: MOSFET driving signal Red:HS to Ground Blue:HB to Ground.
They have met the same problem when 4SBB works in buck mode. But I asked them to increase Cboot or let the power supply more accuracy to solve the prblem
Thank you
Yishan Chen