Hello to all,
I have a question, what is needed, what will work and what shouldn't be done.
My question is regarding correct choosing of components and their order. This is for automotive, and that means it must undergone all of the automotive certifications.
My main concern is regarding surge, transient and reverse polarity protection.
"Case 1" order: Input (13,5V) --> bi-dir TVS --> Schottky diode --> buck converter (12V --> 5V, 3V8, etc.)
"Case 2" order: Input (13,5V) --> Schottky diode --> uni-dir TVS --> buck converter (12V --> 5V, 3V8, etc.)
Is "Case 2" usable in your oppinion? During testing there are all the starting pulses, reverse polarity, transient pulses (ISO 7637-2, ISO 16750-2, etc.).
Thank you in advance.