Other Parts Discussed in Thread: BQ76952, BQ78350-R1A, BQ7830, , BQ34Z100, BQ76940, TIDA-010030, BQ76200, BQ7718
Hi,
I am designing a battery management system for a variety of battery stacks. The stacks will be 4, 10 and 14 cells and I would like to have a single board with population SKU's. The BQ76952 seems to be a very good fit but I also need a fuel gauge. The battery will be about 250Ah so the BQ78350-R1A seemed to be a good fit in terms of capacity.
But looking that the datasheet, it seems as if it is geared to the BQ769x0 family of AFE's. I like the way it interfaced to the AFE via I2C and used the coulomb counter on the AFE and basically seemed to control the AFE. I could use the BQ769x0 but since they come in different package sizes, I would need three PCB's. which is not optimal
Question #1. Can the BQ7830 be used with the BQ76952? And if so, do you have reference schematics?
In another forum regarding the BQ76952, the BQ34Z100-R2 was recommended. This has a different interface and seems to have it's own coulomb counter and shares the sense resistor of the AFE. Seems a little redundant but if it is a good solution and allows me a single PCB, then I can use that. 7000Ah is over kill but again, if it works..
Question #2. Is there a reference design using the BQ34Z100 and the BQ76952?
If there are other solutions for this particular application, I am very open to ideas!!!
Thanks!
John