This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2776: Input voltage

Part Number: LM2776
Other Parts Discussed in Thread: TL7660

I am planning to use  LM2776 for VInput of  5.8V max. The operating ranges states is only 5.5V. but abs max is 6V. Please can you comment if it is okay. 

Please can you also confirm that if TL7660 recommended for new design ?

  • Hi,

    It is not recommended to use LM2776 above the recommended input voltage max of 5.5V.

    Can you please make a new post for TL7660, so that the right product line gets tagged to help you with your questions on that device?

    Best regards,

    Varun