Hi,
For LM51521-Q1, If I set Vout = 16V, if my input using >16V, is it will turn on low side MOSFET to keep Vout = 16V?
Thanks!
Jeff
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
For LM51521-Q1, If I set Vout = 16V, if my input using >16V, is it will turn on low side MOSFET to keep Vout = 16V?
Thanks!
Jeff
Hello Jeff,
The device is not able to keep the output voltage below the input voltage as the backgate diode of the top FET directly connects the input to the output.
So no, the low side FET is off and the high side FET is on to limit losses.
Best regards,
Brigitte
Hi Jeff,
Thank you for using E2E forums, In LM51521 the bypass feature is disabled, meaning when the VIn is one diode drop off voltage above the Vout the device will not go into bypass. In other words, when Vin>Vout+Vf(High side FET's body diode) the device will not go into bypass, which means the high side FET always ON, but instead the high side FET will be off and the Vout will be Vin - Vf(high side FET's body diode). In conclusion to answer your question, no the Low side FET will not be on when your Vin is >16V, but instead you low and high side FET will be OFF and the device will not be boosting and Vout will be equalt to Vin - Vf(body diode of high side FET) so Vout will be Vin - (~0.6)V.
Hope this helps.
BR,
Haroon
Hi Brigitte,
What the difference for LM51521 and LM5152? LM5152 have bypass mode, so means LM5152 will short the body diode to reduce the Vf disapassion?
Thanks!
Jeff