This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ51050B: Would it also charge LiFePo4 ?

Part Number: BQ51050B
Other Parts Discussed in Thread: BQ24072, , BQ25170, BQ25171-Q1, BQ51013B

Hi dear people,

I have a working charging system using a BQ51050B and a BQ24072 to charge a LiPo 1-Cell 500mA battery.

Because of safety reasons, I would like to change to a LiFePo4, 600mA battery.

I wonder if it could be possible to keep the system like it is, by readjusting the charge limiting resistors on both devices.

Are there other considerations that would force me to redesign everything?
The most important is: Would it be possible to have wireless charging?

Best regards

Gustavo