This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: Absolute undervoltage cutoff

Part Number: BQ40Z80

Hello,

I am looking for some clarification on the cell undervoltage levels. Specifically, are there absolute minimums built in that cannot be bypassed? Or is it possible to completely disable the undervoltage cutoff by clearing all the protection and permanent fail bits. Also, it seems that the cell undervoltage threshold (19.10.1.1 of the TRM) can be set to 0mV. So this would also effectively disable the check. Am I interpretting this correctly?

Thank you,

Jamie