Other Parts Discussed in Thread: TPS543A22, TPS543820, TPS54JA20, TPS54KB20
Dear Team,
Do we have suitable solution can meet suggestion which could meet the following requirements?
1-1 The input voltage rating should be higher than 9.2V.
1-2 The efficiency should be higher than 90% for 0.95V out.
1-3 The output current rating should be higher than 7.337A.
1-4 The RθJA specification should be as lower as possible for better thermal performance.
Thank you.
Jimmy