This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3430: TPS3430 WDOG implementation

Part Number: TPS3430

Hi team,

we had integrated tps3430 WWDOG timer, based on configuration:

and calculated tWDU=62.74ms,  tWDL=7ms and tRST=0.70ms. 

I'm implementing code in such a wat that after enabling WDOG using SETx pins(only possible condition is SET0=0,SET1=0), in the while loop generating a pulse with PWM of 50ms signal with86% DC

such that ton=62ms and toff=7ms. Can you guide me is it the correct way of implementing or any approach/Examples  to configure.

Thanks & Regards,

Manikanta Robbi.