Hi team,
Could you answer following questions for quickstart calculator for LM5152-Q1?
(1) For phase margin, could we refer to the margin shown in lower figure (1)? In this case, phase margin is 70~80 degree, correct?
If no, could you share where we need to refer to? (phase margin of 10Hz is 90 degree instead of 0 degree. Could you share why?)
(2) For gain margin, could we refer to the margin shown in lower figure (2)? In this case, gain margin is 30 degree, correct?
(3) How "calculated" RCOMP, CCOMP, and CHF are calculated?
(4) How efficiency curve is calculated?
Regards,
Ochi