Hi TI Team,
We are a battery pack manufacturer and are working on a project that the end product is a battery IP camera (and the battery configuration is cylindrical 21700 1S2P). We are looking for a suitable charger IC that supports 5 LEDs (just to show the power levels by 20%, 40%, 60%, 80% and 100%). Please kindly advise the options of the suitable charger ICs.
The input voltage and current are as the followings (The reason why there are different voltage inputs is because the input sources are to be from different adaptors and solar panels).
1. Voltage: 4.75~5.5V / Current 2A max.
2. Voltage: 5.94~7.26V / Current: 1A max.
3. Voltage: 0~8V / Current 0.2A max.
Thank you.
Louis Cason
Fuji Electronics Group—Taiwan Office
Email: louis.cason@fujielec.com
Company website: www.fujielectronics.com.cn
WeChat/LINE: okaa1414
WhatsApp: 886988787570