Part Number: BQ34Z100
Other Parts Discussed in Thread: BQSTUDIO,
I am having the same error as I've seen in previous threads. I'm using the Evaluation Module which appears to have the bq34z100G1.
I haven't had any issues calibrating the gauge using the bq34z100g1 target.
I can't program the chemistry and I assume the reason is again that the device is showing up as 0100_0_06, which is not on the list of gauges.
I see that I am supposed to "upload the firmware to the device through the programming plugin within BQStudio" to solve this issue.
I am looking at the Firmware. I would think I would need this one, "bq34z100_v2_02_00_31.exe".
However, I look under programming and I see that I need a bqfs file to program.
Am I looking at the wrong thing? Can someone clarify. Is there a document to reference on how to do this?
Thank you in advance.