This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS82130: EMC radiated emissions.

Part Number: TPS82130
Other Parts Discussed in Thread: TPSM82913, TPS62933, TPS62913

Hi, we have a design that operates from +12V in and uses 2 TPS82130 devices to generate both 3.3V and 5V DC supplies.
We have just conducted EMC pre-compliance testing for this design and we are seeing peaks in the radiated emissions at approx. 32MHz and again at 125MHz, very close to the class B limit. Investigations suggest that these wideband peaks are coming from the DC-DC converters. The TPS82130 are highly integrated designs and we have followed the datasheet closely. Is there any recommendation to how we can improve this radiation from the devices, without using additional screening? The PCB is in a plastic box, so there is no screening from the enclosure. I will share a pic of the PSU schematic and EMC plots, one showing a close up the nature of radiation.

 SmartBox PSU schematic.pdf