This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5157: Boost converter IC LM51571RTER not enabling

Part Number: LM5157

Dear TI team,

I am using IC LM51571RTER as boost converter (Input=10 V, Output=20 V). I have applied 1.2 V across Enable pin of IC (Enable threshold is 0.7 V max) but I am not able to turn on Boost IC.

Note: Bias pin voltage=10 V

Thanks,

Shritesh