We're using the RHA version (5962R1222403VXC) with Vout=7V & I_load=530mA.
Question: The curve below applies to 1.8V with I_load =500mA, would this curve also apply to our use case of Vout=7V with I_load=530mA, if not can we get a curve that applies to our use case ?
Note: The curve below was taken from E2E Post Titled: "TPS7A4501-SP: Minimum voltage headroom required for 5V, 100mA operating point."
Thank you -John