Hi team,
I was wondering if there was any limitation or headroom needed between the input voltage and output voltage. Ie if there was a headroom of 0.5V, and Vout is 5.5V, Vin can't be greater than 5V. Is this the case for this part?
Also, is there a pass through feature so that when Vin > Vout, Vout = Vin?
Lastly, this is being used for a non-battery application (5V to 5.5V). Is there any concern with that (datasheet mentions this is for battery-powered applications).
Thanks!
Lauren